Specify the Trace's Source

You use the Trace Properties window (see Configure a Trace) to configure various properties associated with a trace. This section explains how to use the window's Source field to specify a trace's data source. A trace's data source is a database item, such as a point or master station accumulator, that has Historic enabled.