Minimum Configuration

As a minimum, for any type of channel you have to configure these connection-specific properties:

Serial connection

The port to which the channel is connected.

Remote serial connection

The host name of the machine that is running the Port Server application, and the port to which the channel is connected.

TCP/IP connection

The TCP/IP type, the host address, and port number.

Network

The TCP/IP type. (Network configuration is not applicable to PSTN channels.)

If you are configuring a PSTN channel, you also have to enter a telephone number in the appropriate field on the PSTN tab.

For any type of channel, you have to put the channel In Service, and save the configuration if you want the channel to be functional (online).

This will provide a functional channel that uses default configuration settings.