Configuring Advanced EWS Analog Points

Use Advanced EWS Analog Points to map analog ‘point’ data on Advanced EWS servers into Geo SCADA Expert in a suitable format, and vice versa.

Configure the properties of each analog point using the fields on the Advanced EWS Analog Point Form.

This section covers configuration of the analog-specific properties on the Analog Point tab of the Form.

Use the Analog Point tab to:

If the point is an analog output point:

Properties on other tabs are common to many points, see Tabs on Point Forms in the Geo SCADA ExpertGuide to Advanced Drivers.