Advanced Modbus Eavesdropping Arrangement

Eavesdropping allows a new system to run in parallel with an existing system in order to test the new system’s configuration. The Advanced Modbus protocol uses an Rx and Tx eavesdropping arrangement.

While eavesdropping is in progress, any unexpected behavior can be investigated using the Advanced Modbus Eavesdrop logging option see Driver Logging Options that are Specific to the Advanced Modbus Driver.

For more information on eavesdropping, see Using Eavesdropping to Test a New Server’s Configuration.