Configuring Time Points

The Geo SCADA Expert Advanced Modbus driver supports Time points.

On the Advanced Modbus driver, Generic Time Points are currently only supported for use on the Lufkin SAMS driver. That driver is an extension of the Advanced Modbus driver.

Use a Time Point within the Geo SCADA Expert database to retrieve a date/time value from a Modbus device (see Defining Time Point Details in the Geo SCADA Expert Guide To Core Point Configuration).

Configure the properties of each time point using the fields on the Advanced Modbus Time Point Form.

This section covers configuration of properties on the Time Point tab of the Advanced Modbus Time Point Form. The properties on other tabs are common to points on many advanced drivers (see Tabs on Point Forms).

Use the Time Point tab to: