Configuring an Advanced Modbus Channel

The Advanced Modbus driver supports two types of Advanced Modbus channel:

Modbus controllers can communicate with the Geo SCADA Expert server using direct comms or PSTN. With any controllers that communicate using a direct channel but that have a dial-up modem as a ‘backup’ means of contacting the Geo SCADA Expert server, you can configure the controllers to use PSTN as a ‘fallback’ means of communication (see Direct - PSTN Fallback). (In which case, you need to configure a Advanced Modbus PSTN Channel to represent each PSTN line via which the controllers can communicate, in addition to the Advanced Modbus Direct Channel(s).)

In each case, you specify the features for a channel using the fields on the appropriate Advanced Modbus Channel Form.

Each Advanced Modbus Channel Form has several tabs. This section covers configuration of properties that are Advanced Modbus specific. For information on configuring properties that are common to many channels, and for information on tabs not covered in this section, see Tabs on Channel Forms.

Use the fields on the Modbus tab to:

With Direct channels, use the fields within the Scan Groups section of the Scan Parameters tab to specify the frequency with which current data is updated in Geo SCADA Expert (see Define Intervals for Timed Current Data Updates). For ‘Generic’ points (points supported directly by the Advanced Modbus driver, rather than an Extension Driver), the Scan Group interval should be a multiple of the points’ Retrieval Interval rate (see Configure Common Point Properties).