Configure Private Security

Some OPC DA servers support Private Security, whereby you have to log onto the server in order to access the data. Use the Private Security section of the tab to indicate if Private Security is supported, and if so, provide the credentials of a suitable Geo SCADA Expert User Account that provides the required access: