Enable Alarms - Independent Disabled on the Server

The Enable Alarms action allows you to re-instate the alarms and alarm features for an item (that has its alarms currently disabled). But the way in which the Enable Alarms action is applied varies according to whether the Independent setting is enabled or disabled on the server.

In this section, we explain how Geo SCADA Expert applies Enable Alarms when Independent is disabled. For information on how Enable Alarms works when Independent is enabled, see Enable Alarms - Independent Enabled on the Server.

If Independent is disabled on your server, it means that an item’s alarms are enabled as soon as the Enable Alarms action is triggered. Geo SCADA Expert does not consider whether the item’s alarms have been disabled by other Logic programs, users, Schedules, or Method Calls.

So, with Independent disabled:

When the alarm features are re-enabled for an item, Geo SCADA Expert will: