Specify the Characters used for the Alarm Filter Indicators

The filter indicators that display on the Alarm Bell Button can be configured to use characters other than the following defaults:

You can use the Options window's Alarms and Events tab to chose the characters used for the Filtered and Modified indicators.

To define the characters used for the alarm filter indicators:

  1. Log on via a user account that has the Configure Options permission, and then display the Options window.
  2. Select the Alarms and Events tab, and then use the properties in the Indicators section to define the following:
    • Filtered—Enter the character you would like to use to indicate that a filter is applied to the Alarm Banner
    • Modified—Enter the character you would like to use to indicate that a default alarm filter has been modified.

      ATTENTION: If you leave a field blank, the associated filter indicator will not appear on the Alarm Banner Button.

  3. To apply the settings, select the Option window’s OK button.
    Your choices will take effect immediately (on the ViewX client on which you made the changes).