Status

Associated with: CFX Exports

This status attribute indicates the present state of an export request.

The possible states are:

  • Idle—No data export is in progress.
  • Pending—An Export to CFX action associated with this CFX Export database item is awaiting execution.
  • In Progress—An Export to CFX action associated with this CFX Export item is presently under way.
  • Failed—This state indicates that the most recent Export to CFX action was unsuccessful. The status will remain Failed until another export is requested, and then the Status attribute will change to indicate the status of the new action. The cause of the failure will be indicated by an entry in the Alarms List and Alarm Banner (see CFX Specific Alarm and Event Categories).