Failed Third-Party ODBC Client - System Connections

If the third-party ODBC client - system connection cannot be established, the ODBC client will be unable to connect to Geo SCADA Expert.

The connections will fail to establish if:

The third-party ODBC client - system connection works in the same way as a ViewX - system except that it uses a different license and it requires Data Access components (to be installed on the computer that is running the third-party ODBC applications). The firewall rules for third-party ODBC client - system connections are the same as those for ViewX - system connections.