Activities that are Restricted when Configuration or Structure Changes are Pending

Geo SCADA Expert's Configuration Transaction feature is designed to block certain changes to items in Group Templates and Group Instances when updates are pending. This restriction helps to avoid ‘race conditions’. A race condition is where two or more tasks attempt to access the same resource at the same time with unpredictable results. For example, a user could make configuration changes to items in a Group Instance that has updates pending. While the user is making the changes, the update occurs. This causes a race condition as the update and the user are trying to access the same resource at the same time. This can result in the changes made by the user being overwritten by the update.

The Configuration Transaction feature restricts users from performing certain tasks while transactions are pending, including:

To help prevent the most common causes of ‘race conditions’, Geo SCADA Expert uses a pending transactions count. By using this count, Geo SCADA Expert can determine if there are further updates to be applied (see Pending Transaction Count).

The Transactions section of Geo SCADA Expert’s Server Status Tool provides details about any Group Template and Group Instance transactions while those transactions are pending or in progress:

Further Information

Transactions Section of the Server Status Tool: see Transactions in the Geo SCADA Expert Guide to the Server Status Tool.