Add an Item to the Database

To create and configure an item in the database, you need to be logged on via a User Account that:

You also need to be aware of the Database Structure and Database Security requirements of your system, and have undertaken any necessary Preparation.

You can access the database structure within ViewX by using the Database Bar. This is one of the Explorer Bars (see Explorer Bars).

To add an item to the database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the Group, or Group Template within which you want to add the item.
    A context-sensitive menu is displayed.

  3. Select the Create New option.
    A further menu is displayed.

    To add a new Group Instance and associate that Instance with an existing Group Template, you select the Create Instance option, rather than the Create New option. For more information, see Add a Group Instance.

  4. Select the menu option that is appropriate to the item that you want to create:

    To add an item for a particular driver:

    1. Select the appropriate <Driver Name> option (for example, DNP3).
      A further context-sensitive menu is displayed.
    2. Select the type of item that you want to create (for example, a DNP3 Direct Channel).
      An item of the selected type is added to the Geo SCADA Expert database. The entry is highlighted, ready for you to define its name.
    3. Give the item a suitable name (taking into account the Geo SCADA Expert Naming Restrictions).

    For information on the items that are supported by a particular driver and the order in which those items should be configured, see the driver-specific documentation.

    With a few drivers, you select the entries from a different branch of the Create New menu. If this applies, it will be mentioned in the guide for that driver.

    To add a ‘core’ item:

    1. Select the appropriate menu option (for example, select ‘Alarm Redirection’ if you want to add a new redirection action to enable Geo SCADA Expert to redirect alarms).
    2. In some cases, a further menu is displayed—select the appropriate option (for example, ‘E-Mail Action’ to add an e-mail redirection action).
      An item of the selected type is added to the Geo SCADA Expert database. The entry is highlighted, ready for you to define its name.
    3. Give the item a suitable name (taking into account the Geo SCADA Expert Naming Restrictions).

You can then configure the item in the database.

Some Geo SCADA Expert database configuration is carried out using configuration Forms (see Working with Forms). A Form exists for every item in the database. This guide covers those aspects of Form-based configuration that are not specific to a particular driver, along with Basic Configuration Procedures. The Geo SCADA Expert Guide to Point Configuration covers aspects of point configuration that are common to internal points and to points on many drivers.

Many items that you add to a Geo SCADA Expert system will be driver-specific (they are only available if a specific driver, such as the DNP3 Driver, is installed). Refer to the relevant driver-specific guide for information on configuring the driver-specific items in your database, including the order in which you should configure the items in your database.

This Guide to Core Configuration covers configuration of many ‘core’ items, such as Master Station Accumulators, Value Maps, Data Grids, and Schedules—for more information, see Introduction.

You can also configure other ‘core’ items such as: