Define When the Source of a Delta Accumulator has Reset

Use the Source Reset Type combo box on the State tab of the Delta Accumulator Form to specify how the Accumulator detects when its source value has reset:

The options are:

The examples below demonstrate each Source Reset Type and how the selected option impacts on the resulting values of the Delta Accumulator compared to the values of the source from which its values are determined.