Define the Acceptable Number of Alarm Summary Records

Use the AlarmSummary tab on the Root Group Form to enable or disable and define a warning limit for the number of Alarm Summary records that you expect to create per hour. In addition you can set the maximum number of records stored in a granule. Once a granule reaches the maximum size all further records for the granule are discarded.

Use the following fields to enable or disable and define the Alarm Summary record limits:

Severity

Use the Severity combo box to select the Severity Level. This is the severity of the alarm that you want Geo SCADA Expert to display in Alarm Summary messages when the number of records created per hour reaches the number defined in the Warning and Maximum fields. You can disable the alarms by setting the Severity to None, in which case theWarning field is grayed out.

Area of Interest

This field is only displayed if the Area of Interest feature is enabled on your system. Use the field to specify the Area of Interest with which overactive alarms are to be associated (see Assign a Different Area of Interest to an Item's Alarms and Events).

Warning

Enter the number of Alarm Summary records per granule per hour that raise a warning alarm. If the number of records in an individual granule reaches this number an alarm is raised to indicate that the granule is overactive. The minimum value you can enter is 500 records. The default value is 14,400 records/hour (4 records/second for an hour).

This default is provided to avoid false alarms and data loss on large systems.

For this feature to be effective you need to specify values appropriate for your system, to avoid problems before a warning is generated.

The Warning alarm message indicates which granule is overactive including both the time and the filename.

"Too many alarm summary records (# records in hour beginning <time>) file <filename>"

When an alarm is triggered, the alarm source indicates which stream contains the overactive granule (if streams are enabled).

"Alarm Summary (Stream #)"

The Warning field is unavailable and grayed out if the Severity is set to None.

Maximum

Enter the maximum number of Alarm Summary records per granule per hour that can be logged. If the number of records in an individual granule reaches this number an alarm is raised to indicate that the granule has reached the maximum value and no more alarm summary entries will be logged for the objects in this stream for the remainder of this period. The minimum value you can enter is equal to the Warning number of records or 500 if alarms are disabled. The default value is 115,200 records/hour (32 records/second for an hour).


This default is provided to avoid false alarms and data loss on large systems.

For this feature to be effective you need to specify values appropriate for your system, to avoid problems before a warning is generated.

Lowering the maximum number of records below the size of existing granules prevents any further records being added to those granules, it does not affect the existing records in those granules.

The Maximum alarm message indicates which granule was overactive and is now full including both the time and the filename.

"Too many alarm summary records, granule is full (# records in hour beginning <time>) file <filename>"

When an alarm is triggered, the alarm source indicates which stream contains the overactive granule (if streams are enabled).

"Alarm Summary (Stream #)"

If the Severity field is set to None, no alarm is raised when the Maximum number of records is reached.

NOTICE

LOSS OF DATA

When a granule reaches the specified maximum size all further records for the granule are discarded. This will result in the loss of data. To help prevent loss of data, you need to set appropriate maximum values
Failure to follow these instructions can result in loss of data

When Alarm Summary data files (granules) become overactive: