Delete a Scheduled Action

If an action that is associated with a Schedule no longer needs to be triggered by that Schedule:

  1. Display the Schedule in Design Mode.
  2. Either:
    1. Right-click on the action in the Object area of the Schedule Display.
      A context sensitive menu is displayed.

    2. Select the Delete option.

    Or:

    1. Select the action in the Object area of the Schedule Display.
    2. Press the Delete key.

    The obsolete entry is removed from the Schedule Display.

  3. Save the configuration.