Edit a Scheduled Action

To edit an action that is assigned to a Schedule:

  1. Display the Schedule in Design Mode.
  2. Either:
    • Double-click on the action in the Action display area.

    Or:

    1. Right-click on the action in the Action display area.
      A context-sensitive menu is displayed.
    2. Select the Edit option.

      The Edit Action window is displayed.

  3. Use the Edit Action window to perform any of the following:
    • Specify a different database item.
    • Specify a different aggregate.
    • Specify a different alarm association.
    • Specify a different action.
    • Specify the values of any arguments that further define the action.

      For more information on using the window, see Specify a Method.

  4. Save the configuration.