Importing Existing Database Items

You can import database items to replace or update existing database items. When you import a database item into a Geo SCADA Expert database to replace or update an identically named item in that database, Geo SCADA Expert will do the following:

Further Information

The impact of the Exclude From Exclusive Control setting on a Group, Group Template, or Group Instance when adding, copying, or importing database items into that Group, Group Template, or Group Instance: see Copying Database Items when using the Exclusive Control Feature.

Preparation required before importing configuration from one system to another in which custom extra fields (metadata) have been added directly in the past: see Specify the OPC Property.