Logging

Associated with: Channels

The Logging state is indicated by a dark yellow background color, by default.

The color indicates that Communications, I/O, TLS, or Telnet logging is enabled on the channel. When this feature is enabled, the communications between the Geo SCADA Expert server and the outstations that are using the channel are logged to a text file.

For information on channel Communications logging, I/O logging, or TLS logging, see Communications Logging. For information on Telnet logging, see Telnet Monitoring.