Points

Most drivers support a variety of Points. For each input or output value that is associated with plant, you need to create and configure a point of the appropriate type in the Geo SCADA Expert database. For instance, if your Geo SCADA Expert system communicates with outstations using the DNP3 protocol, you would add a DNP3 Point of the appropriate type to your system and associate that point with the input or output data on the relevant DNP3 outstation or other DNP3 device.

You can also add internal points to your system. Such points are not associated with plant, but instead only exist within the master station software. You can use internal points, for example, within Logic programs, or to simulate plant (see Internal Points in the Geo SCADA Expert Guide to Core Point Configuration). Create and configure an internal point on your system if you require such values in the Geo SCADA Expert database and you require any of the following:

For more information on points, see the Geo SCADA Expert Guide to Core Point Configuration.

For driver-specific information on points, see the relevant driver guides.