Specify the Default Map

Use the Default Map Source field on the Geographic Information tab of the System or Root Group to specify the default map that Geo SCADA Expert should use for ad-hoc mapping. For example, to display the location of a database item (see Display On Map in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients). The default map could be a single-layer base map, such as the OpenStreetMap® world map, or a multi-layer composite map. For more about Geo SCADA Expert maps, see About Geo SCADA Expert Maps.

To specify the default map, select the field’s browse button to display a Reference browse window. Select a Map Source or a Map Set from the window. For more about Map Sources and Map Sets, see Creating a Map Source and see Creating a Map Set.