The Effects of Alarm Suppression in Geo SCADA Expert

This section explains the effect that alarm suppression has on Geo SCADA Expert. The effect differs slightly depending on the type of alarm suppression ('By Alarm State' or 'By Expression') and the configuration that is specified on the child database item(s).

(Alarm suppression requirements are configured on the 'child' items (the items on which alarms are to be suppressed), rather than the 'parent' database item (the item that triggers the suppression). This provides greater flexibility by enabling different suppression settings to be set up per child item, even if some of those child items reference the same parent database item.)

Regardless of the type of alarm suppression used, the parent-child alarm relationship can be cascaded, so that when a top level parent item fulfills the suppression criteria it will disable the alarms of its child items, and of the children of those child items, and so on.

For examples that demonstrate the effects of alarm suppression in Geo SCADA Expert, see Example Configuration.

If configuration is imported into the database (in a Geo SCADA Expert .sde file), the value of each imported point is considered NULL on import, so will not be suppressed initially. The effects of any alarm suppression will only come into force when Geo SCADA Expert processes the initial updates for the imported points. For more information about the import process, see Importing and Exporting Database Items.