Define the Historic Export Details

You can use Geo SCADA Expert to export historic point and accumulator data to external historian applications (for example, AVEVA Historian). To do this, you need to enable the storage of historic data for the point or accumulator (see Defining Historic Details for a Point). You then need to specify the historian applications to which you want to export the data. You do this by using the Historic Exports field in the Export section of the Historic tab.

 

Once the Historian or Historic Data Export database item for a historian application has been added to the Historic Exports field, data that is subsequently stored in Geo SCADA Expert's historian will also be exported to that historian application (provided that the Historian/Historic Data Export database item has valid configuration and is In Service). Exported historic data is subject to the same requirements as those for Geo SCADA Expert's historian; namely that each entry must meet the historic storage criteria of the individual point or accumulator. This includes meeting any Compression and/or Historic Data Filter criteria that might be configured for that point or accumulator. For more information see:

Put Aside data is excluded from historic exports.

Data that was already stored in Geo SCADA Expert's historian from before the historian application was added to the Historic Exports field will not be exported to that historian application.

If a Historian/Historic Data Export database item is subsequently placed out of service, data that is added to Geo SCADA Expert's historian during that time will not get exported to that historian application. Once the Historian/Historic Data Export database item is placed back In Service, data export will resume and will include data that is added to Geo SCADA Expert's historian from that moment onwards.