Export the Report in Crystal Reports Format

If Geo SCADA Expert is to export a report in Crystal Reports format, use the Format field on the Export Format tab to specify the Crystal Reports format. The tab displays these fields:

When exported, the report remains in Crystal Reports format. The exported version of the report retains the settings and layout that were specified when the report was last edited (assuming that the specified fonts are available from whichever location the exported report is accessed).