Export the Report in Separated Values Format

If Geo SCADA Expert is to export a report in Separated Value format, use the Format field on the Export Format tab to specify the Separated Value format.

If you are going to export a report in Separated Value Format, only include content in data fields. This is because the export process treats all fields as records and so will export multiple copies of any headers, footers, field titles, and so on.

When the Format is set to Separated Value, the tab displays these fields: