Launch the Crystal Reports Application

To launch the Crystal Reports application from within Geo SCADA Expert, either:

  1. Double-click on the Report entry within the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature).

Or:

  1. Either:
    • Right-click on the Report entry within the Database Bar.

    or:

    • Select the required Report entry on a List.

    or:

    • Select an animated representation of the report on a Mimic.
      A context sensitive menu is displayed.
  2. Select the Edit Crystal Reports option.

The Crystal Reports application window overlays the Geo SCADA Expert window (see Understand the Crystal Reports Work Areas).