Geo SCADA Expert Parameters

You can add Parameter database items to Geo SCADA Expert. You can use such Parameters for storing static data values, such as map grid references. Parameters are internal to Geo SCADA Expert and are designed to store data that is not directly associated with other items in the database (such as individual points, outstations, or scanners). You can use Parameters as an alternative to Custom Configuration Fields, if the values that need storing are not directly associated with other items in the Geo SCADA Expert database.

To include Geo SCADA Expert Parameter data in your reports, you need to either include the Parameters in a Data Grid, or as a subreport (see Use a Subreport to Include Unrelated Data in the Same Report).

For more information on configuring Geo SCADA Expert Parameters, see Using Parameters to Store Static Data Values in the Geo SCADA Expert Guide to Core Configuration.

Do not confuse Geo SCADA Expert Parameters with Crystal Reports’ Parameters (see Parameter Field).