Configure the Scanner Properties

Use the fields on the Scanner tab of the DF1 Scanner Form to define the general and DF1-specific properties for a scanner. Many of the fields on this tab are common to many scanners (see Configuring Scanners on Simple Drivers in the Geo SCADA Expert Guide to Simple Drivers). Those fields that are specific to scanners on the DF1 driver are described below.