Configuring Analog Points

The DF1 driver supports Analog Input and Analog Output points.

Configure the properties of each analog point using the fields on the DF1 Analog Point Form.

This section covers configuration of properties on the DF1 tab of the Form.

Use the DF1 tab to:

For information on the fields on the Analog Point tab, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.