Alarm Limits

Use the fields within the Alarm Limits section of the Analog Point tab to set limits for a DNP3 analog point and specify whether an alarm or event is generated if the point’s value exceeds those limits.

Many of the Alarm Limit fields are common to various types of analog points (see Configure the Limits for an Analog Point in the Geo SCADA Expert Guide to Core Point Configuration). In addition to the usual Limits, DNP3 analog points also have an Invalid state. Use the fields associated with this state to define the properties should the analog to digital conversion process fail in the outstation.

The Alarm Limits section of the tab also includes these fields: