Define the Maximum Size of Data Packets

The DNP3 driver sends and receives data in packets that are known as Frames. For large amounts of information, more than one frame may need to be transmitted.

DNP3 application messages are broken into fragments. The fragment size is determined by the receiving device’s buffer. For systems operating in environments with high levels of interference, communications are often found to be more successful if the fragment size is further reduced.

Use these fields within the relevant DNP3 section of the tool to specify the maximum size of each frame and fragment: