Add a File to a SCADAPack E Outstation’s Configuration

Use the Add button on the Configuration Setup Window to import a file into the Geo SCADA Expert database so that it can be downloaded to the DNP3 SCADAPack E outstation during a configuration download.

To add a file, select the Add button—the Open window (shown below) is displayed.

Use the Open window to browse to and select the file that you want to add to the outstation’s configuration. You can filter the type of file, using the Files of type combo box.

Once you have located the required file, highlight the file entry and select the Open button. The Properties window is displayed. Use the window to specify the properties of the file (see Specify the Properties of a File in a SCADAPack E Outstation’s Configuration).

Once you have specified the file’s properties, select the OK button on the Properties window. The file’s details are added to the Configuration Setup Window.

Select the OK button on the Configuration Setup window to add the specified file to the DNP3 SCADAPack E outstation in the Geo SCADA Expert database.