Configure Network Access Parameters

For multi-drop networks, the SCADAPack E outstation can perform ‘media collision avoidance’, whereby transmissions are checked for collisions with another transmission on the network. If a collision is detected, the outstation re-attempts the transmission, after a delay. The Modes that support collision avoidance are:

Use the fields within the Network Access Parameters section of the SCADAPack tab to define the operational characteristics when a SCADAPack E outstation uses a multi-dropped network, such as a radio network. Specify each value in the OPC Time Format.

If both the Fixed Delay and Max Random Delay are set to zero, the SCADAPack E outstation does not perform any collision avoidance.