Configure any Physical Binary Input Point Properties

Use the fields located at the top of the Input tab on the DNP3 SCADAPack Binary Input Point Form to specify how the SCADAPack E outstation processes the binary point when it has a Point Type of Physical Input (see Configure Common Properties of DNP3 SCADAPack Points).