Configure the Telemetry Computer Properties

Use the fields within the Telemetry Computer Configuration section of the X.29/TC Comms table to specify the connection properties of up to four DNP3 master station servers that are running the X.29 Packet Assembler/Disassembler (PAD) software. The servers are also known as Telemetry Computers (TCs).

For greatest efficiency, enter the most frequently contacted Telemetry Computer’s details in the left-most column, followed by the next most frequently contacted TC, as the X.29 driver processes the entries in order, from left to right.