Create a Mimic to Display the Points

  1. Create a Mimic (for information on creating and configuring a Mimic, see the Geo SCADA Expert Guide to Mimics).
  2. Drag-and-drop the DNP3 SCADAPack Analog Output Point onto the Mimic.
    A context sensitive menu is displayed.
  3. Select the Value option.
    A further menu is displayed.
  4. Select Formatted Value option.
  5. Drag-and-drop the DNP3 SCADAPack Analog Input Point onto the Mimic.
    A context sensitive menu is displayed.
  6. Select the Value option.
    A further menu is displayed.
  7. Select Formatted Value option.
  8. Save the Mimic.
  9. Put the Mimic into Run mode.

Once you have configured the Mimic, you can Power Up the SCADAPack ES Outstation.