Dial In Connects

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve Port Status information.

This status attribute indicates the number of times that the outstation has dialled in successfully using this port.