Quick Start Tutorial

This section provides a guided tour designed to lead you through connecting a SCADAPack Eoutstation to Geo SCADA Expert, then communicating with that outstation using the DNP3 protocol. The procedure is for a SCADAPack ES outstation, however similar steps can be undertaken using other E outstation models.

To perform the procedure, you will need:

Now proceed as follows:

  1. Confirm that the DNP3 and SCADAPack E Server Components are Installed.
  2. Setup a SCADAPack ES Outstation.
  3. Create the Geo SCADA Expert Database Items.
  4. Power Up the SCADAPack ES Outstation.
  5. Control the DNP3 SCADAPack Analog Output Point.