Specify Whether the SCADAPack Outstation is to Detect if an Analog Point has Stopped Changing

Use the fields within the SCADAPack No Change section of the Analog Point tab to specify if the SCADAPack E outstation is to detect whether a DNP3 SCADAPack point’s value is not changing by an expected value often enough.

The SCADAPack No Change properties do not apply to analog points that have a Point Type of Physical Output.