Specify the Type of Status Information that Geo SCADA Expert is to Retrieve

Use the fields on the Status Type tab to specify the type of status information that Geo SCADA Expert is to retrieve from the SCADAPack E outstation: