Trending Inhibited

Associated with: DNP3 SCADAPack Analog, Binary, and Counter points.

This status attribute indicates whether sampling of the point’s data is currently inhibited at the outstation.

Possible states:

  • True (whenever the Disable All Trends pick action or DisableTrending method are used to inhibit Trend sampling)
  • False (whenever Trend sampling is enabled (for instance, through use of the Enable All Trends pick action)).

For more information on Trend sampling, see Configuring DNP3 SCADAPack E Trend Sampler Functionality.