Classes

Classes define the structure of the database and the tables within it. Each class consists of a collection of Fields, Aggregates, and Methods. The structure of a Tables is defined by the classes that form the table.

There are two types of class:

Each class has a base class except CDBObject and CAggregate (the roots of the class hierarchy).The base class is the parent class of the class.

The classes that are base-classes also have sub-classes. The sub-classes are the child classes of the selected class.

You can use the Geo SCADA Expert Database Schema to display information about each class (see Working with the Database Schema).