Configuration Change CRC

Associated with: All items

This status attribute is only displayed if:

  • The Configuration Change CRC feature is enabled on your system
  • The user account with which you are logged on to Geo SCADA Expert is allocated the Configure permission for the selected item (the item for which you are viewing status information).

The Configuration Change CRC value is a cyclic redundancy check (CRC) value that changes whenever the item's writable configuration changes. By comparing the CRC value of an item on an archive, backup, or sde against that of the same item on a 'live' system, a system administrator can determine whether that item's configuration has changed.