Control Feedback Point

Associated with: Analog output points, digital output points and pulse controls for which a feedback point has been configured.

The attribute shows the name of the feedback point associated with the point or pulse control.

For more information, see Configuring Control Checks Settings and see Control Feedback Settings.

Example:

Feedback.Feedback Input