IO Logging
Associated with: Channels on advanced drivers
This status attribute indicates whether Geo SCADA Expert is logging the communications on a channel, including data that was discarded by the driver (see Communications Logging Status in the Geo SCADA Expert Guide to Server Administration).
Possible states:
- Enabled—Logging is in progress on the channel. The logging with cease if the driver or system is shutdown and restarted, or there is a server changeover.
- Enabled (Persist)—Logging is in progress on the channel and will continue after the driver or system has been shutdown and restarted, and after a server changeover.
- Disabled—Logging is deactivated on the channel.
For more information, see Communications Logging in the Geo SCADA Expert Guide to Server Administration.