Last Feedback Timed Out

Associated with: Analog output points, digital output points and pulse controls for which a feedback point has been configured.

Geo SCADA Expert will set the attribute to True if the last feedback period ended without the feedback point receiving an input value that satisfied the check set for the point. Geo SCADA Expert will set the attribute to False when a user issues a new control.

For more information, see Configuring Control Checks Settings and see Control Feedback Settings.

Example:

False