Last Good Outgoing Call

Associated with: PSTN outstations or outstations on which PSTN fallback is enabled

This attribute displays the date and time of the last call to be sent successfully from Geo SCADA Expert to the outstation. The attribute is only displayed once such a call has been made.

Example:

20/Mar/2008 16:48:05.971

Also see the Outgoing Calls attribute, which provides a summary of the outgoing calls since the statistics were last reset.