M/S Alarm Limits

Associated with: Analog Points for which Master Station alarm limits are currently tuned

This status attribute is only displayed for analog points on which:

  • Master Station Alarm Limits are used (see Master Station Alarm Limits in the Geo SCADA Expert Guide to Core Point Configuration)
  • The Tune Limits feature is supported and enabled on those Master Station alarm limits
  • One or more Master Station alarm limits are currently tuned (see Tune M/S Alarm Limits).

The attribute lists:

  • The values to which the Master Station alarm limits are temporarily tuned (the actual number of limits is configurable on a per point basis)
  • The name of the user that was logged onto the workstation when the tuning occurred
  • The date and time that the tuning occurred.
  • Example:

    Tuned to 95.00 90.00 87.00 80.00 20.00 15.00 10.00 5.00 by PMalin at 02/Jun/2008 14:44:47.063
    (For an analog points that has four High and four Low master station alarm limits configured.)

Also see Alarm Limits.