Master-Slave Communications
Most drivers enable Geo SCADA Expert to be the SCADA Master. When the Geo SCADA Expert serveris the master, Geo SCADA Expert initiates and controls the transmissions to and from the other devices on the system.
Some drivers enable Geo SCADA Expert to be a Slave. When Geo SCADA Expert is a slave, the server acts like an outstation and reports any changes to another SCADA master. The SCADA master may be another Geo SCADA Expert server, or a third-party server. When Geo SCADA Expert is a slave, any ‘point’ data is mapped into a simple block of memory in the driver, using a Value Map or Filtered Value Map (see Configuring Value Maps in the Geo SCADA Expert Guide to Core Configuration). The driver-specific documentation specifies which type(s) of Value Map and/or Filtered Value Map a particular slave driver supports.
If a Geo SCADA Expert driver is a slave driver, the word ‘Slave’ is included in the driver name. Drivers that do not include the word ‘Slave’ in their name typically enable Geo SCADA Expert to be the SCADA Master.
With any Geo SCADA Expert driver, refer to the driver-specific documentation for information on which database items you need to configure in Geo SCADA Expert, in order for Geo SCADA Expert to be either the SCADA Master or a Slave.
Be aware that it is possible for Geo SCADA Expert to be both a SCADA Master and a Slave, if both master and slave Geo SCADA Expert drivers are installed on a system.
The
- Geo SCADA Expert Configured as a SCADA Master
- Geo SCADA Expert Configured as a SCADA Slave
- Geo SCADA Expert Configured as both a SCADA Master and a SCADA Slave.
Further Information