Points and Pulse Actions

Geo SCADA Expert uses Points to represent the inputs and outputs in an outstation or similar device. In the database, the values that the outstations receive from plant are stored in input points and the values (controls, and so on) that are sent from Geo SCADA Expert to the plant are stored in output points.

For each input and output, you need to add and configure the type of point that corresponds to the type of protocol and data that Geo SCADA Expert is to read or write from plant.

You configure Pulse Actions to represent those items of plant that you only want to control for brief periods of time (as opposed to output points for those items for which the controlled state is to be maintained).

By performing actions on points and pulse actions, you can interact with the plant. For example, by controlling the state of a digital output point that represents a valve, you could open or close the valve.

The following tables show examples of how points are used in some industries:

Oil, Gas and Petrochemical Pipelines

Digital Input Points Analog Input Points Digital Output Points Analog Output Points Counters

Valve status

Flow level

Valve open/close

Variable valve position

Flow meters

Pump status

Pressure level

Pump start/stop

   

PIG detection

Density level

PIG launch

   

Local/Remote Mode

Temperature

Pipeline shutdown

   

Leak Detected

Tank level indicator

     

Pipe shut-in status

Mass flow rate

     

Batch launched

Leak size

     

Batch arrived

Leak location

     
 

Batch size

     
 

Flow profile

     
 

Pressure profile

     
 

Temperature profile

     
 

Pipeline efficiency

     
 

Instrument accuracy

     
         

Entries in italics are generated by third party Leak Detection software. Geo SCADA Expert uses computed digital input points and computed analog input points to represent these items.

Oil and Gas Gathering and Production

Digital Input Points Analog Input Points Digital Output Points Analog Output Points Counters

Valve status

Inlet/Outlet pressure

Valve open/close

Variable valve position

Flow meters

PIG detection

Temperature level

PIG launch

   
 

Pressure level

     
 

Flow rate

     
 

Energy flow rate

     
 

Gross calorific value

     
 

Mass flow rate

     

Water Treatment

Digital Input Points Analog Input Points Digital Output Points Analog Output Points Counters

Valve status

Inlet tank level

   

Flow meters

Pump status

Inlet flow rate

     

Air blower status

Turbidity level

     

Centrifuge status

Chlorine level

     

Power supply
status

pH level

     
 

Clean/dirty tank level

     
 

Sludge tank level

     
 

Carbon level/
dosage

     
 

Aluminum level

     
 

Sulfuric acid level/dosage

     
 

Phosphoric acid level/dosage

     
 

Lime level/
dosage

     

Flood Forecasting and Environment

Digital Input Points Analog Input Points Digital Output Points Analog Output Points Counters

Penstock status

Weir level

     

Valve status

Rain gauge

     

Pump status

River level

     

Intruder alarm

River
temperature

     

Power supply
status

       

Power Generation and Distribution

Digital Input Points Analog Input Points Digital Output Points Analog Output Points Counters

Phase indication

Input/output voltages

     
 

Input/output
current

     

Further Information

For information on configuring specific types of point and pulse action, see the relevant driver guide.

For general information on points, pulse actions and their configuration, see the Geo SCADA Expert Guide to Core Point Configuration.

Actions Associated with Points.

Actions Associated with Pulse Actions.